This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PLC电力载波中集中器收不到表端模块数据和表端模块收不到集中器下发命令疑问



您好:

        我们在使用集中器配合表端模块收发数据稳定性测试时发现有两种现象,一种现象为 集中器向表端模块发送要数据命令时收到了确认信息11 00 00 24 02 80 00 20 02 00 00 02 00 08 02 01 00 02 00 01 02 10 00 02 00 07 02 70 00 04 00 00 01 00 02 40 00 02 00 00,但是在表端模块的PLC板串口处却没有收到集中器下发的要数据命令,另一种现象为表端模块收到了集中器下发的要数据命令并且响应回复数据后表端模块PLC板串口处收到确认信息00 00 10 00 73 03 00 00 02 00 01 08 07 00 00 00 00 00 00 00,但是集中器确收不到表端模块回复的数据。以上出现的情况每隔几分钟就会出现一次,其他时间收发数据正常,想问一下出现这种情况可能会是什么原因?我们电力线上用的直流110V

  • 对于现象1:比较难断定,因为不确定是DC发出来表没有收到还是DC没有发出来。不知道你们有没有电力线sniffer,可以用附件中的sniffer测试下看看电力线上有没有数据发出来(请注意该sniffer用起来可能有些bug,某些情况下每用一次需要重新烧一次固件),或者试着增大发送间隔看看能不能解决问题,或使出现问题的机会减小。

    对于现象2:不知道表端host在发出数据后,能收到模块反馈的确认信息吗?如果能的话可能也需要检查下电力线上的信息。

    wireshark_prime_sniffer.zip