This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS编译FLASH后出现若干warning,不知原因



描述如下

 

Description Resource Path Location Type creating output section "PieCtrlRegsFile" without a SECTIONS Example_F2802xECap_Capture_Pwm    C/C++ Problem creating output section "PartIdRegsFile" without a SECTIONS Example_F2802xECap_Capture_Pwm    C/C++ Problem creating output section "NmiIntruptRegsFile" without a SECTIONS Example_F2802xECap_Capture_Pwm    C/C++ Problem creating output section "I2caRegsFile" without a SECTIONS Example_F2802xECap_Capture_Pwm    C/C++ Problem creating output section "SysCtrlRegsFile" without a SECTIONS Example_F2802xECap_Capture_Pwm    C/C++ Problem creating output section "SpiaRegsFile" without a SECTIONS Example_F2802xECap_Capture_Pwm    C/C++ Problem creating output section "SciaRegsFile" without a SECTIONS Example_F2802xECap_Capture_Pwm    C/C++ Problem creating output section "PieVectTableFile" without a SECTIONS Example_F2802xECap_Capture_Pwm    C/C++ Problem entry-point symbol other than "_c_int00" specified:  "code_start" Example_F2802xECap_Capture_Pwm    C/C++ Problem creating output section "XIntruptRegsFile" without a SECTIONS Example_F2802xECap_Capture_Pwm    C/C++ Problem creating output section "SysPwrCtrlRegsFile" without a SECTIONS Example_F2802xECap_Capture_Pwm    C/C++ Problem creating output section "DevEmuRegsFile" without a SECTIONS Example_F2802xECap_Capture_Pwm    C/C++ Problem creating output section "ECap1RegsFile" without a SECTIONS Example_F2802xECap_Capture_Pwm    C/C++ Problem creating output section "CsmPwlFile" without a SECTIONS specification Example_F2802xECap_Capture_Pwm    C/C++ Problem creating output section "CsmRegsFile" without a SECTIONS Example_F2802xECap_Capture_Pwm    C/C++ Problem creating output section "EPwm3RegsFile" without a SECTIONS Example_F2802xECap_Capture_Pwm    C/C++ Problem creating output section "EPwm4RegsFile" without a SECTIONS Example_F2802xECap_Capture_Pwm    C/C++ Problem creating output section "EPwm1RegsFile" without a SECTIONS Example_F2802xECap_Capture_Pwm    C/C++ Problem creating output section "EPwm2RegsFile" without a SECTIONS Example_F2802xECap_Capture_Pwm    C/C++ Problem creating output section "FlashCallbackVar" without a SECTIONS Example_F2802xECap_Capture_Pwm    C/C++ Problem creating output section "FlashRegsFile" without a SECTIONS Example_F2802xECap_Capture_Pwm    C/C++ Problem creating output section "EmuBModeVar" without a SECTIONS Example_F2802xECap_Capture_Pwm    C/C++ Problem creating output section "EmuKeyVar" without a SECTIONS specification Example_F2802xECap_Capture_Pwm    C/C++ Problem creating output section "GpioDataRegsFile" without a SECTIONS Example_F2802xECap_Capture_Pwm    C/C++ Problem creating output section "GpioIntRegsFile" without a SECTIONS Example_F2802xECap_Capture_Pwm    C/C++ Problem creating output section "FlashScalingVar" without a SECTIONS Example_F2802xECap_Capture_Pwm    C/C++ Problem creating output section "GpioCtrlRegsFile" without a SECTIONS Example_F2802xECap_Capture_Pwm    C/C++ Problem creating output section "AdcRegsFile" without a SECTIONS Example_F2802xECap_Capture_Pwm    C/C++ Problem automatic RTS selection:  linking in "rts2800_ml.lib" in place of index Example_F2802xECap_Capture_Pwm    C/C++ Problem creating output section "Comp1RegsFile" without a SECTIONS Example_F2802xECap_Capture_Pwm    C/C++ Problem creating output section "AdcResultFile" without a SECTIONS Example_F2802xECap_Capture_Pwm    C/C++ Problem creating output section "CpuTimer0RegsFile" without a SECTIONS Example_F2802xECap_Capture_Pwm    C/C++ Problem creating output section "Comp2RegsFile" without a SECTIONS Example_F2802xECap_Capture_Pwm    C/C++ Problem creating output section "CpuTimer2RegsFile" without a SECTIONS Example_F2802xECap_Capture_Pwm    C/C++ Problem creating output section "CpuTimer1RegsFile" without a SECTIONS Example_F2802xECap_Capture_Pwm    C/C++ Problem

  • 您好,

    可能是因为使用的 cmd 文件不对,请问工程中所使用的 cmd 文件名称是什么?

  • 我碰到的问题如下:

    <Linking>
    warning #10247-D: creating output section "PartIdRegsFile" without a SECTIONS specification
    'Finished building target: SVPWM.out'

    cmd文件是:

    28335_RAM_lnk.cmd
    DSP2833x_Headers_nonBIOS.cmd

    请问该如何解决?谢谢!

  • 解决了

    在DSP2833x_Headers_nonBIOS.cmd中添加了

     PARTID      : origin = 0x3D7E80, length = 0x000001     /* Part ID register location */

    /*** Device Part ID Register Structures ***/
       PartIdRegsFile    : > PARTID,   PAGE = 1
    参看帖子http://www.deyisupport.com/question_answer/microcontrollers/c2000/f/56/t/72333.aspx