This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我用TI自带的28069的HRPWM的例程,发现端口没有脉冲产生,我仔细核对了一下TI提供的SPRUH18D(讲诉3HRPWM的技术文档)中给的关于HRPWM的说明与例子,发现对HRPWM的初始化都是相同的,现在一直没找到原因在哪里,求助啊啊?????????????现在把程序贴出来,供各位解读!
#include "F2806x_Device.h" // F2806x Headerfile
#include "F2806x_Examples.h" // F2806x Examples Headerfile
#include "F2806x_EPwm_defines.h" // useful defines for initialization
void HRPWM1_Config(int);
void HRPWM2_Config(int);
void HRPWM3_Config(int);
void HRPWM4_Config(int);
Uint16 i,j, DutyFine, PeriodFine ,n,update;
Uint32 temp;
void main(void)
{
InitSysCtrl();
InitEPwm1Gpio();
InitEPwm2Gpio();
InitEPwm3Gpio();
InitEPwm4Gpio();
DINT;
InitPieCtrl();
IER = 0x0000;
IFR = 0x0000;
InitPieVectTable();
update =1; DutyFine =0; PeriodFine =0;
EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0;
EDIS;
HRPWM1_Config(10); // ePWM1 target, Period = 10
HRPWM2_Config(20); // ePWM2 target, Period = 20
HRPWM3_Config(10); // ePWM3 target, Period = 10
HRPWM4_Config(20); // ePWM4 target, Period = 20
EALLOW;
EPwm1Regs.HRPCTL.bit.HRPE = 1; //Enable High resolution EPwm1 period
EPwm2Regs.HRPCTL.bit.HRPE = 1; //Enable High resolution EPwm2 period
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1; //Enable TBCLKSYNC
EDIS;
while (update ==1) //测试微调HRPWM的占空比,精度可以达到0.02%
{
for(DutyFine =1; DutyFine <256 ;DutyFine ++) {
// Example, write to the HRPWM extension of CMPA
EPwm1Regs.CMPA.half.CMPAHR = DutyFine << 8; // Left shift by 8 to write into MSB bits
EPwm2Regs.CMPA.half.CMPAHR = DutyFine << 8; // Left shift by 8 to write into MSB bits
// Example, 32-bit write to CMPA:CMPAHR
EPwm3Regs.CMPA.all = ((Uint32)EPwm3Regs.CMPA.half.CMPA << 16) + (DutyFine << 8);
EPwm4Regs.CMPA.all = ((Uint32)EPwm4Regs.CMPA.half.CMPA << 16) + (DutyFine << 8);
for (i=0;i<10000;i++){} // Dummy delay between MEP changes
}
}
void HRPWM1_Config(period)
{
EPwm1Regs.TBCTL.bit.PRDLD = TB_IMMEDIATE; // set Immediate load,立即装载TBPRD寄存器的值
EPwm1Regs.TBPRD = period-1; // PWM frequency = 1 / period 设置周期值
EPwm1Regs.CMPA.half.CMPA = period / 2; // set duty 50% initially,设置占空比
EPwm1Regs.CMPA.half.CMPAHR = (1 << 8); // initialize HRPWM extension EPwm1Regs.CMPB = period / 2; // set duty 50% initially
EPwm1Regs.TBPHS.all = 0; EPwm1Regs.TBCTR = 0;
EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP; //向上计数方式
EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE; // EPwm1 is the Master
EPwm1Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_DISABLE; //disable EPWMxSYNCO signal
EPwm1Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; //TBCLK的时钟等于系统时钟
EPwm1Regs.TBCTL.bit.CLKDIV = TB_DIV1;
EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;
EPwm1Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;
EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
EPwm1Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
EPwm1Regs.AQCTLA.bit.ZRO = AQ_SET; // PWM toggle low/high
EPwm1Regs.AQCTLA.bit.CAU = AQ_CLEAR;
EPwm1Regs.AQCTLB.bit.ZRO = AQ_SET;
EPwm1Regs.AQCTLB.bit.CBU = AQ_CLEAR;
EALLOW; EPwm1Regs.HRCNFG.all = 0x0;
EPwm1Regs.HRCNFG.bit.EDGMODE = HR_REP; //MEP control on Rising edge
EPwm1Regs.HRCNFG.bit.CTLMODE = HR_CMP; //选择CMPAHR寄存器和TBPRDHR寄存器控制 the edge position
EPwm1Regs.HRCNFG.bit.HRLOAD = HR_CTR_ZERO;
EDIS;
}
其他的HRPWM的配置都是和HRPWM1的配置相同,这里把void InitEPwm1Gpio(void)的代码页贴出来:
void InitEPwm1Gpio(void)
{
EALLOW;
GpioCtrlRegs.GPAPUD.bit.GPIO0 = 1; // Disable pull-up on GPIO0 (EPWM1A)
GpioCtrlRegs.GPAPUD.bit.GPIO1 = 1;
GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 1; // Configure GPIO0 as EPWM1A
GpioCtrlRegs.GPAMUX1.bit.GPIO1 = 1; // Configure GPIO1 as EPWM1B
GpioCtrlRegs.GPADIR.bit.GPIO0 = 1;
EDIS;
}
请各位帮忙找找问题在哪,在GPIO0管脚始终没有PWM脉冲,GPIO1和其他的都没有!我通过延时程序可以在GPIO0处产生PWM波,硬件上应该没有什么问题,不知道是不是哪里设置有问题!
我提到的可以在GPIO0处产生PWM是将其设置成IO端口,利用延时让其端口电平翻转产生PWM,而不是用利用特殊功能产生的!时钟是设置好了的!在InitSysCtrl()函数里面, 这个函数里面主要是IntOsc1Sel()和InitPll(DSP28_PLLCR,DSP28_DIVSEL)以及InitPeripheralClocks()函数来设置时钟的,采用的是internal oscillator 1,频率为10MHZ,程序如下:
void IntOsc1Sel (void)
{
EALLOW;
SysCtrlRegs.CLKCTL.bit.INTOSC1OFF = 0;
SysCtrlRegs.CLKCTL.bit.OSCCLKSRCSEL=0; // Clk Src = INTOSC1
SysCtrlRegs.CLKCTL.bit.XCLKINOFF=1; // Turn off XCLKIN
SysCtrlRegs.CLKCTL.bit.XTALOSCOFF=1; // Turn off XTALOSC
SysCtrlRegs.CLKCTL.bit.INTOSC2OFF=1; // Turn off INTOSC2
EDIS;
}
然后通过InitPll(DSP28_PLLCR,DSP28_DIVSEL)函数将系统时钟设置为80MHZ,而InitPeripheralClocks()函数就是设置外设时钟的,程序如下:
void InitPeripheralClocks(void)
{
EALLOW; // LOSPCP prescale register settings, normally it will be set to default values
GpioCtrlRegs.GPAMUX2.bit.GPIO18 = 3; // GPIO18 = XCLKOUT
SysCtrlRegs.LOSPCP.all = 0x0002; // XCLKOUT to SYSCLKOUT ratio. By default XCLKOUT = 1/4 SYSCLKOUT
SysCtrlRegs.XCLK.bit.XCLKOUTDIV=2; //对系统时钟进行四分频
SysCtrlRegs.PCLKCR1.bit.EPWM1ENCLK = 1; // ePWM1
SysCtrlRegs.PCLKCR1.bit.EPWM2ENCLK = 1; // ePWM2
SysCtrlRegs.PCLKCR1.bit.EPWM3ENCLK = 1; // ePWM3
SysCtrlRegs.PCLKCR1.bit.EPWM4ENCLK = 1; // ePWM4
SysCtrlRegs.PCLKCR1.bit.EPWM5ENCLK = 1; // ePWM5
SysCtrlRegs.PCLKCR1.bit.EPWM6ENCLK = 1; // ePWM6
SysCtrlRegs.PCLKCR1.bit.EPWM7ENCLK = 1; // ePWM7
SysCtrlRegs.PCLKCR1.bit.EPWM8ENCLK = 1; // ePWM8
SysCtrlRegs.PCLKCR0.bit.HRPWMENCLK = 1; // HRPWM
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1; // Enable TBCLK within the ePWM
SysCtrlRegs.PCLKCR1.bit.EQEP1ENCLK = 1; // eQEP1
SysCtrlRegs.PCLKCR1.bit.EQEP2ENCLK = 1; // eQEP2
SysCtrlRegs.PCLKCR1.bit.ECAP1ENCLK = 1; // eCAP1
SysCtrlRegs.PCLKCR1.bit.ECAP2ENCLK = 1; // eCAP2
SysCtrlRegs.PCLKCR1.bit.ECAP3ENCLK = 1; // eCAP3
SysCtrlRegs.PCLKCR0.bit.ADCENCLK = 1; // ADC
SysCtrlRegs.PCLKCR3.bit.COMP1ENCLK = 1; // COMP1
SysCtrlRegs.PCLKCR3.bit.COMP2ENCLK = 1; // COMP2
SysCtrlRegs.PCLKCR3.bit.COMP3ENCLK = 1; // COMP3
SysCtrlRegs.PCLKCR3.bit.CPUTIMER0ENCLK = 1; // CPU Timer 0
SysCtrlRegs.PCLKCR3.bit.CPUTIMER1ENCLK = 1; // CPU Timer 1
SysCtrlRegs.PCLKCR3.bit.CPUTIMER2ENCLK = 1; // CPU Timer 2
SysCtrlRegs.PCLKCR3.bit.DMAENCLK = 1; // DMA
SysCtrlRegs.PCLKCR3.bit.GPIOINENCLK = 1; // GPIO input clock
SysCtrlRegs.PCLKCR3.bit.CLA1ENCLK = 1; // CLA1
SysCtrlRegs.PCLKCR0.bit.I2CAENCLK = 1; // I2C
SysCtrlRegs.PCLKCR0.bit.SPIAENCLK = 1; // SPI-A
SysCtrlRegs.PCLKCR0.bit.SPIBENCLK = 1; // SPI-B
SysCtrlRegs.PCLKCR0.bit.SCIAENCLK = 1; // SCI-A
SysCtrlRegs.PCLKCR0.bit.SCIBENCLK = 1; // SCI-B
SysCtrlRegs.PCLKCR0.bit.MCBSPAENCLK=1; // McBSP-A
SysCtrlRegs.PCLKCR0.bit.ECANAENCLK=1; // eCAN-A
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1; // Enable TBCLK within the ePWM
EDIS;
}
这里面就有使能EPWM的时钟和HRPWM的时钟设置啊!我在想是不是和SF0_V6.h和SFO_TI_Build_V6b.lib有关,因为这个HRPWM的产生与MEP_ScaleFactor有关,我看TI提供的文档说,这个设置TI提供了SF0_V6.h和SFO_TI_Build_V6b.lib来帮助用户自动完成设置,但是我不知道这个在主程序里还有如何设置啊,我只是把这两个文件添加到了工程当中,并没有在主函数里进行其他的任何操作!
上面建议如果不使能高精度,正常的ePWM能输出吗?有测试过吗?
如果把下面两句话注释掉呢?为什么单独拿出来而未放在ePWM初始化里?有了解高精度周期模式有什么特别注意事项呢?
对比4.2.3.4.1 High-Resolution Period Configuration检查一下看看?
EPwm1Regs.HRPCTL.bit.HRPE = 1; //Enable High resolution EPwm1 period
EPwm2Regs.HRPCTL.bit.HRPE = 1; //Enable High resolution EPwm2 period
如果仍有问题,看看ePWM的计数器是否正常在计数,还有你自己提到的两个库文件可以先删除。
10# 说:上面建议如果不使能高精度,正常的ePWM能输出吗?有测试过吗?
如果把下面两句话注释掉呢?为什么单独拿出来而未放在ePWM初始化里?有了解高精度周期模式有什么特别注意事项呢?
对比4.2.3.4.1 High-Resolution Period Configuration检查一下看看?
EPwm1Regs.HRPCTL.bit.HRPE = 1; //Enable High resolution EPwm1 period
EPwm2Regs.HRPCTL.bit.HRPE = 1; //Enable High resolution EPwm2 period
如果仍有问题,看看ePWM的计数器是否正常在计数,还有你自己提到的两个库文件可以先删除。
为什么对上面两句话视而不见呢?!
有没有阅读一下手册看看下面这句话与你提到的两句话是什么关系?
是否有了解高精度有三种模式:占空比,相位和周期,而周期模式要求特别严格,有很多的注意事项,如上所述?
EPwm1Regs.HRCNFG.bit.CTLMODE = HR_CMP;