This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SCI 稳定通信最大波特率



HI,我们使用F28027,测试中发现能够稳定通信的最大波特率是115.2K bps,每次发送20个字节数,使用中断接收。另一方是PIE的单片机。

如果波特率设置为200K以上,都存在个别字节丢失现象,但是没有乱码,而且SCIRXST的bit7经常会置为1。 使用FIFO接收也有这个问题。

 

所以我想问这个是28027的硬件特性决定了最大波特率还是我的设置有问题?

另外,请问有没有性价比高的、SCI FIFO支持32级深度的 DSP,稳定通信波特率可以达到1M左右?

谢谢