This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
安装CCS5.4后,编译、下载都通过了,但编译后有一个warnings如下:
This project was created using a version of compiler that is not currently installed: 5.2.1 [C2000]. Another version of the compiler will be used during build: 6.1.3. Please install the compiler of the required version, or migrate the project to one of the available compiler versions by adjusting project properties.
不知如何处理,怕运行中有问题,请帮忙解决一下,谢谢!