This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TI-RTOS的疑问

您好!我想请教下几个关于TI-RTOS的问题。

1、我想知道TI-RTOS系统的运行机制。之前我学的一直是ucos-2这个操作系统,这个系统是基于不同优先级任务的,每个任务都是一个while(1)循环,分为单次执行的任务、周期性执行的任务和事件触发的任务。在非单次执行的任务来说,必须调用延时或等待事件的系统服务函数,以给低优先级任务执行的机会。

那TI-RTOS是不是也是这个机制?如果两者是一样的话,学起来就方便了许多。

2、我是在F28m35的M3侧移植了操作系统,因为该芯片还有C28另一个核,那么我能否从C28给M3中传递信号量呢(因为我觉得C28已在TI-RTOS系统的外部了)?

3、在TI-RTOS中一般用mailbox来传递数据,那么我从共享RAM中给TI-RTOS系统任务传递数据要用什么呢?因为共享RAM也可以看成属于C28的了。同样的,我如何把AD采样的数据通过在M3中的采样任务传递到共享的RAM中呢?