您好!
1、我在看在F28M35中移植TI-RTOS的例子,发现所有的project中都没有像未移植系统的例子那样,对PLL、M3、C28的时钟进行了配置。在未移植系统的例子中,有下面的程序语句:
// Sets up PLL, M3 running at 100MHz and C28 running at 100MHz
SysCtlClockConfigSet(SYSCTL_USE_PLL | (SYSCTL_SPLLIMULT_M & 0xA) |
SYSCTL_SYSDIV_1 | SYSCTL_M3SSDIV_1 |
SYSCTL_XCLKDIV_4);
而在TI-RTOS中没有相关的配置语句。这是为什么呢?
2、因为我需要在C28中也要添加工程,那么是不是在m3中加配置C28时钟的语句?是不是也要在M3的TI-RTOS的系统中添加启动C28的语句,如下:
// Send boot command to allow the C28 application to begin execution
IPCMtoCBootControlSystem(CBROM_MTOC_BOOTMODE_BOOT_FROM_FLASH);
3、我要在RAM中开辟空间,那么我如何保证开辟的位置是在共享的RAM中还是在各自的RAM中呢?