This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC7724和DSP28335在用外部接口的情况怎么连线?

Other Parts Discussed in Thread: DAC7724

我这两天做了一个DAC7724的模块,想用DSP28335的外部接口直接控制DAC7724芯片,我知道12跟数据线和2跟地址线、片选线、读写线分别对应相连,那么DAC芯片的LADC和RESET连DSP的哪两根引脚?

  • 楼主,可以选用两个IO口进行控制,LADC主要作用是当其为低电平时,四个输出通道都处于Transparent模式,而当前为高电平时,可以根据A0,A1,RW,CS的状态来选择某个输出通道的寄存器为Transparent或者readback模式,建议仔细阅读datasheet的第14页来了解这几位的功能,至于RESET,其功能就是置低时复位所DAC内部寄存器。

  • 我现在就是直接用两个普通的IO口来控制LDAC和RESET,但是程序下载进去后我是只让A通道输出,可是得到的去测的话每个通道都是-10V,这个是怎么回事?

  • 楼主,关于DAC7724的具体细节问题,你可以在模拟与混合信号的数据转换器板块进行提问,相信这样会让你更快的解决对于DAC部分芯片的问题,C2000这边的硬件连接应该没有问题了。