This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PLC组网时表端模块节点丢失疑问



您好:

1、一个集中器下面挂了6个表端模块,短距离(不超过5米)正常组网通信,电力线上110V直流电压,表端模块程序版本采用V7610,在运行了大概两天两夜即48小时之后出现了丢失其中一个表端模块节点,大概54小时之后又丢失一个表端模块节点即在集中器上看不到这两个表端模块了,另外的4个表端模块节点还在正常与集中器通信,想问一下造成表端模块节点丢失的原因可能有哪些?

2、表端PLC板自身的里面的程序如果复位了会不会造成节点丢失?如果会造成节点丢失那么我们通过Get System Info是不是也可以知道节点断开了?(通过对比Get System Info信息和我们自身Load System Config中的一些信息)

3、对于通过SET_MAC_PIB和GET_MAC_PIB可以知道表端模块网络是否正常,对于文档中提到的 PRIME Spec v1.3E这个文档从哪个地方可以找到?