规格书上说TMS320F280049C的ADC管脚有24个,但实际好几个都是共用的。有没有24个ADC脚完全各自独立的DSP?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
实际上是有25个的,因为有两个引脚属于不同的Analog Group,所以之前多数了两个,不好意思。
规格书上说的23个,应该是因为有两个引脚与GPIO复用,不是单独的模拟引脚,所以他没有算。
看一下是否可以满足您的需求
there are dedicated pins for B5 (pin 32) and B11 (pin 30) which respectively also
have AIO252 and AIO251 functionality. In addition, GPIO20 (pin 48) and GPIO21 (pin 49) are also available as
B5 and B11 respectively. Since B5 and B11 are dedicated pins on this package, it is recommended to use them
instead of the ones on GPIO20/21.
弄得人都不敢下手了
是的,没错,pin32和pin30是B5和B11的专用引脚,pin48和pin49是复用的。
看一下这两个,是有独立的24个外部通道:
375这个我也看了,176pin的abcd各6/4/3/5,再额外两个,总共也才20个
我指的是337引脚的;
针对F280034,那两根线分别接32脚和接48脚,会分别采集这两根线上的电压吗?
可以