关于TIDM_1000的三相交流输入,套件本身定义频率最大值为110Hz,最小值为40Hz。将最大频率改为150Hz或者200Hz是否可以?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
好的,还有一个问题,就是现在整流器运行Bulid1和Bulid2能够实现升压操作,在建立Bulid3时,即添加电压环,ClearTrip=1后。总线电压跳动后又恢复二极管整流输出,无法实现升压操作输出。请问什么原因导致?
Hi lihao,
已经跟进过去了,有了结果我会第一时间回复。
关于整流器的负载,手册上为500欧姆,是否可以为110欧姆,相当于增大输出功率
Hi lihao,
build2如果正常的话,意味着电流环工作正常。build3只是有一个额外的电压环。我们的工程师认为您需要再次检查一下输出电压检测。
我们假设您没有修改TIDM-1000的原始代码,对吗?
关于整流器的负载,手册上为500欧姆,是否可以为110欧姆,相当于增大输出功率
理论上是可以的,看一下这个帖子:TIDM-1000: Minimum load?
关于电压环的问题已经解决。我现在调整稳定电压400V,负载110欧,BULID2电流环无法在ClearTrip=1时,升压整流操作无法实现,是因为负载太低的缘故吗?
补充下,我给定交流输入相电压50Vrms,整流稳定电压400V,负载值110,建立Build2后,清除跳闸ClearTrip=1,电流环升压无法达到400V,请问是什么原因导致。我给定负载500,相电压50Vrms,整流稳定电压400V,Build2在清除跳闸后正常升压。
Hi lihao,
请遵循用户手册中的测试流程。
您可以查看一下TZFLG.OST是否被置位。我们的工程师推测可能因为某些原因,这触发了保护。