This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F20827,F28035新手请教一些问题。



1,开始实时调试的时候,有的项目会提示:

Do you want to enable realtime mode?
Can't enter realtime mode unless debug events are enabled.
Bit 1 of ST1 must be 0.

这个该怎么设置。

2,这两个芯片如果要扩展RAM应该怎么处理?有没有参考的原理图。

3,哪个系列的DSP芯片ADC相对比较可靠一点?

4,

  • 实时调试需要在CCS5版本中用,点击小闹钟按钮能使能。

    这两个芯片都没有外部存储器接口,不能外扩RAM。

    Picolo的ADC是12位的,效果挺好的,如果需要提高精度可以增加offset校准等。