This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP芯片问题

请问:TMS320LF2406APZA 其中的每一个字母代表什么意思?是否有这方面完整的中文学习资料!望各位大佬多多指教!!谢谢!!

  • 例如:TMS320F2812PGFA

    1.前缀:TMX=实验器件 ; TMP=原型器件 TMS=合格器件

    2.系列号:320=TMS320系列

    3.引导加载选项:(B)

    4.工艺:

    C=COMS

    E=COMS  ;EPROM

    F=Flash ; EEPROM

    LC=低电压CMOS(3.3V)

    LF=Flash ; EPROM(3.3V)

    VC=低电压CMOS(3V)

    5.器件类型:

    20x DSP

    24x DSP

    55x DSP

    62x DSP

    3X DSP

    6.封装类型:

    PAG=64 -引脚塑料TQFP

    PGE=144 -引脚塑料TQFP

    PZ=100 -引脚塑料TQFP

    7.温度范围:(默认0°C-70°C)

    L=0°C~70°C

    A=-40°C~85°C

    S=-40°C~125°C

    Q=-40°C~85°C,Q100 Fault Grading

    这么晚还在学习啊?希望对你有所帮助哈!