Part Number: TMDSCNCD28388D
您好:
我打算通过以太网烧录28388的控制程序有两个疑惑
1.想问一下Boot Mode中flashboot和sci boot有什么区别呢?
2.想问下28388通过以太网烧录程序在理论上是否可行?大致思路是咋样呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMDSCNCD28388D
您好:
我打算通过以太网烧录28388的控制程序有两个疑惑
1.想问一下Boot Mode中flashboot和sci boot有什么区别呢?
2.想问下28388通过以太网烧录程序在理论上是否可行?大致思路是咋样呢?
Hi yeyuan zhu,
1. flashboot,代码在flash中,运行flash中的代码;
sci boot,使用bootrom通过sci先将flash kernal烧录到目标器件的RAM中(因为bootrom只能对RAM进行操作),然后flash kernal再将用户代码烧写到flash中。
(sprabv4e_Serial Flash Programming of C2000 Microcontrollers (Rev. E))
(zhcaai4e_C2000微控制器的串行闪存编程 (Rev. E))
2. 理论上可以,但您需要自己写boot,TI的bootrom不支持。
有关这款器件的boot,可以看一下spruii0d_TMS320F2838x Real-Time Microcontrollers With Connectivity Manager TRM (Rev. D) Chapter 5 ROM Code and Peripheral Booting