Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE
TMS320F28379D 双核CPU
1.串口烧录时如果要用Boot1模式,是否需要配置?
2.GPIO28,GPIO29串口烧录,Boot1 SCI模式下,是否可以直接烧录两个核的代码?如果不可以,想问下解决办法?
3.IAP升级时,是否需要写两份bootloader?是否有相关例程供参考?
4.C2000WARE\C2000Ware_4_01_00_00\driverlib\f2837xd\examples\cpu1\dac例程,这个例程是否在CPU2里也可以用,我移植到CPU2后,DAC没有输出,是我配置有问题还是CPU2不能用,如果CPU2不能用,是否有可供CPU2运行的DAC例程?
注:CPU2 DAC代码如下,移植自上述目录例程:
void Init_DAC(void)
{
//
// Set VDAC as the DAC reference voltage.
// Edit here to use ADC VREF as the reference voltage.
//DAC_setLoadMode(DACB_BASE, DAC_LOAD_SYSCLK);
//
DAC_setReferenceVoltage(DACA_BASE, DAC_REF_ADC_VREFHI);
//
// Enable the DAC output
//
DAC_enableOutput(DACA_BASE);
//
// Set the DAC shadow output to 0
//
DAC_setShadowValue(DACA_BASE, 1000);
//
// Delay for buffered DAC to power up
//
DEVICE_DELAY_US(100);
}
int main(void){
Init_DAC();
while(1)
{
DAC_setShadowValue(DACA_BASE, 1000);
DEVICE_DELAY_US(2);
}
return 0;
}