This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我使用TI的SysConfig一次性配置了多个外设,8个epwm,16个ADCA的SOC。编译报错说内存问题,在memory allocation视图下,初步可以认为是因为.text.1太大,而cmd所连接的内存分区太小而导致的编译报错。我知道这种报错如何修改,只是在回顾曾经写的bug日志有了更多的思考。
对此我有以下两个个疑问。
1. 我使用的ram_cmd进行链接的,该文件所指明的text分区放在RAMLS0、RAMLS1、RAMLS2、RAMLS3、RAMLS4中,但很明显RAMLS2并没有完全使用,RAMLS3、RAMLS4甚至没有写入任何东西,为什么这里提到的这个.text.1反而fail placement?
2. .text分区中的内容是可执行代码和常量,那.text.x的意义是什么呢?如图中的RAMLS0下的.text.2,RAMLS1下的.text.3和RAMLS2下的.text.4。
<Linking>
"../cmd/28004x_generic_ram_lnk.cmd", line 76: error #10099-D: program will not fit into available memory, or the section contains a call site that requires a trampoline that can't be generated for this section. placement with alignment/blocking fails for section ".text" size 0x186b page 0. Available memory ranges:
RAMLS0 size: 0x800 unused: 0x0 max hole: 0x0
RAMLS1 size: 0x800 unused: 0x0 max hole: 0x0
RAMLS2 size: 0x800 unused: 0x7ab max hole: 0x7ab
RAMLS3 size: 0x800 unused: 0x800 max hole: 0x800
RAMLS4 size: 0x800 unused: 0x800 max hole: 0x800
error #10010: errors encountered during linking; "Project00-ProjectTemplate-2022-12-27 13-01-27.out" not built
>> Compilation failure
makefile:185: recipe for target 'Project00-ProjectTemplate-2022-12-27 13-01-27.out' failed
gmake[1]: *** [Project00-ProjectTemplate-2022-12-27 13-01-27.out] Error 1
makefile:181: recipe for target 'all' failed
gmake: *** [all] Error 2
**** Build Finished ****