在controlSUITE 中有 28069 的原理图文件,可是尝了几种方法没打开
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请您在此下载:
但是ti在controlsuite里面提供的不是.pcb文件,而是一个.dsn文件和一个叫Gerbers的文件夹,里面给了一个readme的文本文件,内容如下:
Company Name: TEXAS INSTRUMENTS
PC Board Name: F2803x controlCARD
PC Board Number: F2083x
Revision: 1.0
Design House: Willow Spring Technical Services, Corp.
Designed by: Carl Sangiolo
Contact Number: (508) 947 - 2709
e-mail: clsangiolo@comcast.net
Files Included:
Filename Description Format
-------- ----------- ------
L1.PHO Primary Side Cu Gerber 8.5
L2.PHO NEG PLANE Gerber 8.5
L3.PHO PWR PLANE Gerber 8.5
L4.PHO Secondary Side Cu Gerber 8.5
PSS.PHO Primary Silkscreen A/W Gerber 8.5
SSS.PHO Secondary Silkscreen A/W Gerber 8.5
PSM.PHO Primary Soldermask A/W Gerber 8.5
SSM.PHO Secondary Soldermask A/W Gerber 8.5
PST.PHO Primary Solder Stencil A/W Gerber 8.5
SST.PHO Secondary Solder Stencil A/W Gerber 8.5
DD.PHO Drill Drawing Gerber 8.5
NC_DRILL.DRL NC Drill Data NC DRILL ASCII
NC_DRILL.REP Drill Tool Listing ASCII
NC_DRILL.LST Drill X-Y Listing ASCII
IPCD356.NET IPC-D-356 Netlist IPC-D-356 ASCII
README.TXT This File ASCII
NOTES:
1) USE FILM OUTLINE CORNERS TO ALIGN ARTWORKS
2) ALL THERMALS ARE O.D. I.D.= O.D. - .020
WITH A .015 OPEN AT 45 DEGREES.
3) ALL VIAS SHALL HAVE A DIRECT CONNECTION
TO THE PLANE. NO THERMALS ON VIAS.
这些文件明显就无法用expresspcb读取
哦,是这样的,
如果是DSN文件,是原理图,要用OrCad打开,16.2 就行。
此文件夹下没有PCB的原件,只有最后加工的Gerber文件。
TI一般用OrCad for SCH, PADs for PCB, expressPCB for both SCH and PCB
我想下载small PCB antenna的封装,在2540的USB dongle中下载了设计文件,然后文件后缀是.SPL,,请问用什么软件可以打开,或者如何才能转成Altium Designer的封装,非常期待您的回答!
您好!
请问2.4G small PCB antenna封装在哪里下载?可以在CC2540的USB Dongle的设计文件中下载吗?如果是的话需要用什么软件才能打开下载的文件,非常期待您的回答!
不是很确定,因为不同的产品线使用的工具可能不一样,请到无线连接 » 蓝牙Bluetooth 技术论坛去提问:
http://www.deyisupport.com/question_answer/wireless_connectivity/bluetooth/f/103.aspx