This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我在高压电机开发套件上实验无传感器的PMSM电机驱动,在LEVEL1的选项下,按说明书一步一步操作,希望显示说明书上的驼峰正弦波。我开了“Enable silicon real_time Mode"\"Enable polite real_time Mode"以及相应的"Continue Reflesh"按钮。能看到Expressions窗口上的有些数字在实时变化;波形显示满后图形就不动了,好象没有更新。这是怎么回事?
我没有用桌面软件Gui。CCS刚熟起来,CCS已经很不顺利,不想费精力再去搞一个桌面软件Gui。
一开始时能看到波形更新,但波形“满”了后就不变化了。我用Memory Broswer窗口看DLOG_4CH_buff1数组的内容是变化的。
另外还有一个不解的问题:我在打开Graph时用Import导入Graph1.graphProp文件Graph 属性窗口的内容根本没有变化,必须得手动输入Start Address A和Start Address B。是Graph1.graphProp这个文件没用还是我操作有问题?
装CCS4就是问题多,一会儿这个问题一会儿那个问题的。装了三台电脑,重装了不知多少次,都有问题。后来听入说可能同电脑内原先安装的软件有关,我这几台都装有MICROCHIP的MAPLAB IDE。不知道是不是这个关系?过几天换个全新的电脑试试看。现在CCS5还算稳定,你的意思是用CCS4就会解决这个问题?
有个小细节,不知是否有关:装了CCS5后编译提示CGT的版本不对(同上次提问的问题正好相反,这次默认的V6.0.1不行,要选V5.2.10才行)。
今天我买了一个新电脑,装WIN7旗舰版操作系统。安装了CCS5和CONTROLSUITE使用后其它都正常,就是“我在打开Graph时用Import导入Graph1.graphProp文件Graph 属性窗口的内容根本没有变化,必须得手动输入Start Address A和Start Address B。是Graph1.graphProp这个文件没用还是我操作有问题?”这个问题还是老样的。
我用的就是win7 的32位旗舰版, CCS5其他功能都正常,就是想看事实数据,graph 这一个菜单,直接就是灰色的 不让操作。我郁闷啊 ,。那个有这方面的经验。说一说
taotao,
Solution:
Clean the workspace: CCSv4 stores various information in a folder called '.metadata' located in the user's workspace. The contents of this folder can get corrupted over time, causing various instability and strange behavior. Cleaning the workspace often helps resolve these issues. The simplest way to do this is to delete the '.metadata' folder in the workspace. This will essentially reset the workspace and restore the environment to the default behavior. All projects that were in the workspace will need to be re-imported into CCSv4, even though they are still physically in the workspace folder. Also note that any modified preference settings will be lost (set back to the default setting).
If you wish to avoid resetting those preferences, export the preferences to a file (outside the workspace) by selecting 'File->Export...->General->Preferences->To preference file' before deleting the workspace. Once the workspace has been cleaned, those preferences can be imported back into CCSv4 by selecting 'File->Import...->General->Preferences->From preference file'
如果你打开的graph窗口较多的话,有可能出现调试界面速度变慢的问题,如果CCS调试速度没有影响,那么请关闭CCS尝试将workspace 下面路径下的所有内容删除,然后打开CCS,重新添加变量到Graph窗口试一下
C:\workspace\.metadata\.plugins\com.ti.dvt.graph.visualization\savedSolutions
liming 你好,
我用的CCS5.2,在显示变量的时候如何调成图形呢?
我点tools->graph->single time 之后,出现个对话框"the chosen operation is not currently available"