This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F2812串口加载程序



F2812串口加载程序时要求DSP上电复位时从SCIA启动(即要求GPIOF4,GPIOF12复位时为低电平,GPIOF2,GPIOF3复位时为高电平),其中GPIOF4有内部上拉电阻,其它三个引脚没有内部上下拉。我想硬件设计时将GPIOF2和GPIOF3各接4.7K的上拉电阻接到3.3V,GPIOF12接2.2K的下拉电阻接GND,请问这三个引脚这样接行吗?还有第四个引脚GPIOF4同时还是RS232串口的TXD引脚,要怎么接才能使复位时为低电平,复位后又不影响串口加载程序呢?接下拉电阻吗,应该接多大的电阻,具体怎么算?复位之后下载程序时不会影响到232串口程序加载吧?还有这个引脚的内部上拉电阻是多少,内部上拉在该引脚设置为输入输出时都起作用吗?具体在该引脚设置为输入和输出时分别起什么作用?谢谢了,水平比较菜。

  • 您好!

    关于F2812的SCI烧写,TI有官方历程和文档,检索号: spraaq2

    另外建议,将那四个需要跳线的GPIO,接成跳线的形式,否则以后要从Flash Boot会有麻烦。

    此四个GPIO默认都是内部上拉,你只需要将某个GPIO做成跳线即可。