This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP28069中ConfigCpuTimer()函数问题



 我使用的F2806x_CpuTimers.c文件中的标准函数

void ConfigCpuTimer(struct CPUTIMER_VARS *Timer, float Freq, float Period)
{
 Uint32  PeriodInClocks;

 // Initialize timer period:
 Timer->CPUFreqInMHz = Freq;
 Timer->PeriodInUSec = Period;
 PeriodInClocks = (long) (Freq * Period);
 Timer->RegsAddr->PRD.all = PeriodInClocks - 1; // Counter decrements PRD+1 times each period

 // Set pre-scale counter to divide by 1 (SYSCLKOUT):
 Timer->RegsAddr->TPR.all  = 0;
 Timer->RegsAddr->TPRH.all  = 0;

 // Initialize timer control register:
 Timer->RegsAddr->TCR.bit.TSS = 1;      // 1 = Stop timer, 0 = Start/Restart Timer
 Timer->RegsAddr->TCR.bit.TRB = 1;      // 1 = reload timer
 Timer->RegsAddr->TCR.bit.SOFT = 0;
 Timer->RegsAddr->TCR.bit.FREE = 0;     // Timer Free Run Disabled
 Timer->RegsAddr->TCR.bit.TIE = 1;      // 0 = Disable/ 1 = Enable Timer Interrupt

 // Reset interrupt counter:
 Timer->InterruptCount = 0;

}

程序执行时在变量窗口里面看不到Timer->RegsAddr->PRD.all 的值?单步执行时会直接跳过Timer->RegsAddr->PRD.all = PeriodInClocks - 1;这一步,好像这一步没执行,我用的系统时钟频率80M,调用函数时设置Freq值为40, Period值为8000,用的80管脚的28069片子