C2000的FLASH写入有很多种方式。我现在采用的是TI的API库完成代码的下载。但是TI的API库消耗的系统RAM比较多。
编译后大家可以看到Map的分配文文件。尤其是在容量较小的C2000的芯片中。我载入API库后发现,API需要消耗0x521个RAM
空间,而28027中RAM空间比较小,这样分配后,系统可用RAM更少了。
所以我想请教一下专家,C2000的FLASH的擦写过程是什么样的。具体要怎么操作。包括需要操作那些寄存器。类似于8位的MCU一样,
可以通过汇编等高效语言编写一个API库,一个可以节省一些RAM空间,二可以为后期的其余型号C2000的MCU服务。