This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello各位,在HVPM_sensorless-2833x例程中,会有一些基值参数需要针对不同的电机进行设置:
#define BASE_CURRENT 10 // Base peak phase current (amp)
#define BASE_TORQUE // Base torque (N.m)
#define BASE_FLUX // Base flux linkage (volt.sec/rad)
基电流的设置是按照电机的额定电流进行设置吗?
我的电机功率是400W,3000r/min,2.8A,是不是我的BASE_CURRENT 要设置成2.8呢,这样的话标么化之后1才代表2.8A,不会对电机有危险
但是电机启动加速过程电流应该是很大的,额定电流的好几倍,这样的话电流值就升不上去,会导致电机不能启动么
麻烦各位解释下