This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ccs5 调试问题

Other Parts Discussed in Thread: CONTROLSUITE

刚会用ccs5建立工程

code_start:
    .if WD_DISABLE == 1
        LB wd_disable       ;Branch to watchdog disable code
    .else
        LB _c_int00         ;Branch to start of boot.asm in RTS library
    .endif

在 LB wd_disable这里走不出去了,什么情况?

  • 您好,

    应该是工程文件不完整导致的,建议您从 controlSUITE 中的示例代码开始入门。能否将工程文件列表的截图贴出来?

  • wd_disable是一个函数,具体停在那个语句中:

    wd_disable:
        SETC OBJMODE        ;Set OBJMODE for 28x object code
        EALLOW              ;Enable EALLOW protected register access
        MOVZ DP, #7029h>>6  ;Set data page for WDCR register
        MOV @7029h, #0068h  ;Set WDDIS bit in WDCR to disable WD
        EDIS                ;Disable EALLOW protected register access
        LB _c_int00         ;Branch to start of boot.asm in RTS library

        .endif

    这段代码正常不会有等待的地方,建议下载一个TI的demo程序先验证硬件等正常。