This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28027上电串口接收报错



问题在“F28027串口FIFO收发中断问题”有描述。


写到flash后,重新上电,串口接收报错,导致无法接收数据,发送正常。
报错:寄存器SCIRXST-RX ERROR 1,寄存器SCIRXBUF-SCIFFFE/SCIFFPE 1

按一下复位按钮,接收就正常了。这是啥情况哦??有兄弟碰到过没有?
串口初始化代码:
void InitSci(void)
{
  // Initialize SCI-A:
  SciaRegs.SCICCR.all = 0x0007;   // 1 stop bit,  No loopback
                                  // No parity,8 char bits,
                                  // async mode, idle-line protocol
  SciaRegs.SCICTL1.all = 0x0003;  // enable TX, RX, internal SCICLK,
                                  // Disable RX ERR, SLEEP, TXWAKE
  // Disable RXRDY/BRKDT/TXRDY interrupt
  SciaRegs.SCICTL2.bit.TXINTENA = 0;
  SciaRegs.SCICTL2.bit.RXBKINTENA = 0;

  SciaRegs.SCIHBAUD = 0x0000;
  SciaRegs.SCILBAUD = SCI_PRD;   // 38400

  // FIFO enable configure
  SciaRegs.SCIFFTX.all = 0xC020;
  SciaRegs.SCIFFRX.all = 0x0021;
  // Disable FIFO interrupt
  SciaRegs.SCIFFTX.bit.TXFFIENA = 0;
  SciaRegs.SCIFFRX.bit.RXFFIENA = 0;
  SciaRegs.SCIFFCT.all = 0x00;

  SciaRegs.SCICTL1.bit.SWRESET = 1;     // Relinquish SCI from Reset
  SciaRegs.SCIFFTX.bit.TXFIFOXRESET = 1;
  SciaRegs.SCIFFRX.bit.RXFIFORESET  = 1;
}