最近使用到了28035的CLA问题,有个关于ADC的问题,我将ACQPS设置为6,根据TI ADC DATSHEET 可知,采样窗口为7,转换时间为13,此外,还在需要2个时钟的延迟,才能将结果存入ADC结果寄存器中,现在问题是如果使用CLA,这20个时钟时间会节省多少?请交与各位高手。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
最近使用到了28035的CLA问题,有个关于ADC的问题,我将ACQPS设置为6,根据TI ADC DATSHEET 可知,采样窗口为7,转换时间为13,此外,还在需要2个时钟的延迟,才能将结果存入ADC结果寄存器中,现在问题是如果使用CLA,这20个时钟时间会节省多少?请交与各位高手。
同意楼上的回复。
请参考CLA UG中"ADC Early Interrupt to CLA Response"部分的说明,使用early interrrupt可以让CLA或CPU在13个ADCCLK转换过程的开始就提前触发中断(而不是默认的转换结束后才触发),从而并行地进入任务或中断,等到ADC转换完成就能立即读取结果。
也可以在数据手册中查看该时序 Figure 6-29. Timing Example for Sequential Mode / Early Interrupt Pulse.
你可以在中断中直接调用结果寄存器的值就可以,我是这么应用的。
比如:
Volt_Adc = AdcMirror.ADCRESULT1 ;