This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bootloader



1.当TRST=1时,Emulator Connected Determine Boot Mode Based on 2 RAM Locations (EMU_KEY andEMU_BMODE),

连接仿真器时,启动模式基于RAM地址(EMU_KEY andEMU_BMODE),EMU_KEY= 0x55AA ,EMU_BMODE怎么设置啊?

EMU_KEY andEMU_BMODE 在哪里设置的啊?

 Boot Mode:   EMU_KEY        EMU_BMODE
//                   (0xD00)         (0xD01)
//      ---------------------------------------
//      Wait         !=0x55AA        X
//      I/O          0x55AA          0x0000
//      SCI          0x55AA          0x0001
//      Wait         0x55AA          0x0002
//      Get_Mode     0x55AA          0x0003
//      SPI          0x55AA          0x0004
//      I2C          0x55AA          0x0005
//      OTP          0x55AA          0x0006
//      Wait         0x55AA          0x0007
//      Wait         0x55AA          0x0008
//      SARAM        0x55AA          0x000A   <-- "Boot to SARAM"
//      Flash        0x55AA          0x000B
//      Wait         0x55AA          Other

当TRST=0时,Emulator Not Connected Determine Boot Mode Based on 2 GPIO Pins and 2 OTP Locations(OTP_KEY and OTP_BMODE)

仿真器不连接时,启动模式取决于2 GPIO Pins 和2 OTP Locations,OTP_KEY and OTP_BMODE在什么地方设置的啊?

2. 利用仿真器向CPU写程序时,需要短接CPU管脚吗?以前用瑞萨时,烧录程序时,需要短接管脚。

我用的是28035.谢谢!

  • 选择【Release】。右键【28035_RAM_lnk.cmd】文件,在出现的菜单中的【Exclude File(s) from Build】选项,使文件【28035_RAM_lnk.cmd】在Release模式下无效。

    在Release模式下编译工程,按上述方法进入调试环境。单击打开图标,加载Release模式下的out文件。这时代码不是加载到RAM中,而是下载到Flash,也就是实际烧写程序

     

     

  • 1.

    EMU_KEY & EMU_BMODE located in PIE at 0x0D00 & 0xD01, respectively

    OPT_KEY & OTP_BMODE located in OTP at 0x3D78FE & 0x3D78FF, respectively

    其实建议您直接通过改变GPIO34和GPIO35的上下拉状态,来更改boot的方式。

    2. 不需要。