This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于CLA协处理器的问题请教.



F28062和F28069的一个很大的区别是062没有CLA,而069有.  但062也有FPU单元,这样的话是不是062处理浮点数据速度不会那么快?

  • 需要了解的是CLA和C28x内核是两个不同的计算单元,CLA作为协处理器可以单独编程使用。

    如果是只用到C28x+FPU的话,那么两个型号的06x在处理浮点运算的能力是一样的。

    如果是用到CLA的话,那么CLA会对芯片整体的运算能力有很大的帮助。

  • CLA相当于是独立于C28X内核的另外一个内核,而062和069在其本身C28X内核的性能上是一样的。只是069的总体处理能力会因为增加了一个CLA而上升