请问controlSUITE里的HVPSFB套件用得F28027,我现在改用28035.那个PCMC里的文件F28027_FLASH_HVPSFB.CMD应该怎么修改一下?我没作修改就连接XDS100烧写F28035导致28035之后再也连接不上了。其他的冠名2802x的头文件之类的,我都换成2803x的头文件了,编译也是只有一个警告的。请问还有哪些要注意的吗
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问controlSUITE里的HVPSFB套件用得F28027,我现在改用28035.那个PCMC里的文件F28027_FLASH_HVPSFB.CMD应该怎么修改一下?我没作修改就连接XDS100烧写F28035导致28035之后再也连接不上了。其他的冠名2802x的头文件之类的,我都换成2803x的头文件了,编译也是只有一个警告的。请问还有哪些要注意的吗
1. 请问加密了么?除非密码区的128bit全部加密,正常情况下,不可连接是不正常的。
2. CMD文件的修改,可以参考TI历程中的F28027和F28035CMD的差别,主要是一些Ram和Flash区的分配的不同。
3. 您是否已经换成了F28035的硬件?还是依然用的F28027的硬件,用的F28035的程序?
我是看28035和28027的存储器的地址和大小都是向上兼容的,cmd文件我就没做修改了,结果就杯具了。
现在再烧录调试时就提示片上存储器错误了。
后来我对照了一下28027和28035的flash的cmd文件,发现28027是从flashA加载到progRAM的,而28035是从flashD加载的。
我都是直接用controlSUITE里的HVPSFB套件得程序,他们没有做加密的吧。
硬件我是完全改用28035了,我就是想评估一下28035里面的用于实现数字电源的峰值电流模式控制的比较器模块的。