This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于2808的ADC使用问题?



这两天在调2808的ADC时,发现外面输入电压在1.13V以上时很好,采样值很线性,但低于1.13V后采样值突然就跳变了,从1.13V直接跳变到1.03再变到0.93。但实际外面输入电压并未跳变。但到了0.93V以下又线性了,不知道为什么?跟踪了结果寄存器,值的确是跳变了,不是程序问题,请高手解决一下?
  • 从时间上确保转换结果对应的确实是该时刻的外部输入电压,另外如果使用软件触发,通过实时模式观察此时的结果寄存器看看是否有其它影响?

    也可以直接使用TI的例程测试一下。