This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28M35H52C1 到底有没有问题?



前面用 XF28M35H52C1 做的板子,调通了程序,也生产了几套样品。现在买到的是F28M35H52C1芯片,焊在以前成熟的板子上。调试发现出现以下问题:

1.以太网不通(在XF28M35上调试通过的 ,YF-AV24D3W)

2.SDRAM 读写不了(在XF28M35上读写没问题)

3.FLASH 没法烧写(在XF28M35上烧写没问题)

还有其它的一些功能暂时没测试,不清楚TI芯片F28M35H52C1RFPT (YFB-39AE0SW)到底有没有问题。

  • 哦,顺便说一下,我看了一下F28M35的勘误表,里面更改功能的管脚和我的电路没关系,也就是说,里面的部分管脚功能更不更改和我的电路没关系,因为压根我就没用到哪些更改的功能。另外我的芯片版本是 “B"。

  • zhenhua,

    参照下面的帖子

    http://e2e.ti.com/support/microcontrollers/c2000/f/171/t/251698.aspx

    If you have received Rev A/Rev B samples of Concerto devices, the attached XML files will need to be placed in the following Code Composer directory in order to enable programming:   These XML files will also work with Rev 0 silicon.

    <CCS install directory>\ccs_base\c2000\nowFlash\configs.

    4426.xml_update.zip

    If you are using UniFlash, the updated xmls should go to: uniflashv2\ccs_base\c2000\nowFlash\configs.

    Alternatively, you can install device support updates from CCS5 help menu (check for updates) and these latest xmls will be placed at ccsv5\ccs_base\c2000\nowFlash\configs.  But for UniFlash, these xml files have to be manually placed at above mentioned Uniflash path for now.  We will work to update the UniFlash installer to include the latest xml files.

    edit: The above files are for CCS V5.