This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
InitAdc(); 进入这个函数后运行ADC延迟函数 DELAY_US(ADC_usDELAY); 延迟函数为: .def _DSP28x_usDelay .sect "ramfuncs" .global __DSP28x_usDelay_DSP28x_usDelay: SUB ACC,#1 ///////从这个位置跳转到中断函数 BF _DSP28x_usDelay,GEQ ;; Loop if ACC >= 0 LRETR
中断函数为: interrupt void USER1_ISR(void) // User Defined trap 1 { // Insert ISR Code here // Next two lines for debug only to halt the processor here // Remove after inserting ISR Code asm (" ESTOP0"); for(;;); }
新手 不解 请各位高手支招
xiangpu,
F28035.cmd是否是controlSUITE中的例子?C:\ti\controlSUITE\device_support\f2803x\v127\DSP2803x_common\cmd
如果是,应该CMD没有问题。
如果使用flash的CMD,程序会烧写到flash中执行,那么应该在程序中要初始化flash,参考C:\ti\controlSUITE\device_support\f2803x\v127\DSP2803x_examples_ccsv5\flash_f28035 例程。
应该要程序编译后的相关警告信息,如果有,贴出来帮助判断。
Eric