把28003x_generic_ram_lnk.cmd更换为28003x_generic_flash_lnk.cmd并编译烧录程序后,仿真不了并且断电重新上电后,开发板没有跑示例程序,可以判断开发版flash中默认的程序被擦除了,但是也没有跑烧录后的程序,想问一下如何烧录程序到flash中并成功跑起来?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
把28003x_generic_ram_lnk.cmd更换为28003x_generic_flash_lnk.cmd并编译烧录程序后,仿真不了并且断电重新上电后,开发板没有跑示例程序,可以判断开发版flash中默认的程序被擦除了,但是也没有跑烧录后的程序,想问一下如何烧录程序到flash中并成功跑起来?
使用的是led_ex1_blinky这个例程,开发板是LAUNCHXL_F280039C,在device.h中新增加了#define _LAUNCHXL_F280039C 宏定义,
然后使用28003x_generic_ram_lnk.cmd编译仿真可以运行,更换为28003x_generic_flash_lnk.cmd编译烧录之后就不能仿真了,而且断电再重新上电也不跑flash中的程序
导入例程后不需要对例程做任何代码上的修改,通过下述步骤即可将程序修改为烧录到FLASH中并从FLASH运行:

然后编译-->debug/Flash,并确保boot开关处于正确位置即可。
Hi chusanqian,
例程中的build configuration不是新建完工程就有的,需要人为配置。
project-->properties:

那您这边有新建工程配置为烧录到flash中的build configuration配置方法吗?目前我新建工程只有RAM的。