This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSHVMPPTKIT开发套件的平台搭建问题



TMDSHVMPPTKIT开发套件包含两个部分,DC-DC和DC-AC,我们小组现在的方法是采用5个60V/5A的开关电源串联模拟太阳能电池板给DC-DC提供不小于230V/500W的输入,通过调整其中一个开关电源的电压大小模拟太阳能光线转换,不知道这么搭建平台是否合理?希望相关人员和设计爱好者能够给出宝贵的建议

  • guotao,

    请问你们是想实现MPPT的功能,还是只想实现逆变的功能?

    如果只想实现逆变的功能的话,那么采用直流源+DC/AC的板子就可以了。

    如果也想实现MPPT,建议还是用PV source或是输入光伏阵列。

    建议先调完MPPT再跳DC/AC。

    Eric

  • Dear Ma,

    感谢你的回复,起码我们小组在这方面有些信息了。不过我还有个问题,您所提到的PV source我们应该去哪里购买,光伏阵列的有效率与标识和我们现有的不符。举个例子,一般的光伏板和模拟太阳能电池500W的PV输出电压基本不会高于200V,而这块板子的DC-DC需要PV输出电压在200V到300V之间。我们究竟如何在实验室条件下实现MPPT功能,有没有好的建议,或者渠道能够帮助我们找到解决现在实验平台搭建的有效方法,多谢!