This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28035CLA任务计算结果错误



在使用28035CLA时,使用2806X的sqrt范例,选择使用C28XX发现程序停留在Cla1ForceTask1andWait();无法进行下一步。

选择使用CLA0,得到的数据不对。已经选择配置支持cla0

编译器型号为6.1.5

2803x.cla如下所示:

#include "DSP28x_Project.h" #include "CLAMath.h" #include "CLAShared.h"

//Task 1 : Calculate sqrt(X) interrupt void Cla1Task1 ( void ) {    __mdebugstop();     fResult = CLAsqrt(fVal); }

 

请各位帮忙解答下,谢谢。

 

 

补充说明下:

针对上边错误,加入Cla1Regs.MIER.all = M_INT11;这一句后问题解决。

         但是task1 计算结果错误。相对于范例,我多加了CLAsqrt.asm文件,在该文件中多添加定义了一个_Cla1Prog_Start:。如果去掉这个asm文件,会提示缺少_Cla1Prog_Start:和CLAsqrt定义。添加上计算是错误的。求解释,谢谢。

 

 

再补充下:

    去掉CLAsqrt.asm后,加入CLAmath.lib,并且添加设置include option,在主函数中定义下_Cla1Prog_Start,后,缺少_Cla1Prog_Start:和CLAsqrt定义错误解决,但是经过CLA计算结果全是0.0,结果错误,不知道哪里出问题了,求各位大神解释下,谢谢

 .

CLAsqrt.asm