This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

着急上火啊!专家们帮解决下问题!



1.新买的高压套件F28069M做ACIM性能测试,我先用LAB02A做电机参数测试,测出电感值为1.4*10-7;Rs:0.0256.这值是绝对不对啊,测试很多次有时差别还很大。然后运行电机,不能正常运行。电机参数如下:380V/50HZ  功率:550W。说明:开发板直流电压只加到300VDC.我只验证频率为20HZ时的性能。

LAB02A程序修改如下:

#define USER_IQ_FULL_SCALE_FREQ_Hz        (25.0)

#elif (USER_MOTOR == My_Motor)
#define USER_MOTOR_TYPE MOTOR_Type_Induction
#define USER_MOTOR_NUM_POLE_PAIRS (2)
#define USER_MOTOR_Rr         (NULL) 
#define USER_MOTOR_Rs        (NULL)
#define USER_MOTOR_Ls_d    (NULL)
#define USER_MOTOR_Ls_q     (NULL)
#define USER_MOTOR_RATED_FLUX      (0.8165*380.0/50.0)
#define USER_MOTOR_MAGNETIZING_CURRENT    (NULL)
#define USER_MOTOR_RES_EST_CURRENT    (0.15)
#define USER_MOTOR_IND_EST_CURRENT     (NULL)
#define USER_MOTOR_MAX_CURRENT (3.0)
#define USER_MOTOR_FLUX_EST_FREQ_Hz (5.0)

把电机参数修改成经过别的变频器测试的参数后,电机可以正常运转,但是,电机声音发的声音沉闷,电机参数经过反复修改,均解决不了问题。是不是TI这个方案有缺陷。求解解决办法!!!!!!