This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于28035 CLA的一个问题



最近在搞一个程序(程序中在RAM中调试),用到了CLA,遇到了个问题,我在main.c文件中定义如下:

#pragma DATA_SECTION(God, "Cla1ToCpuMsgRAM");

volatile float God;

在TSAK8中完成初始化,如下所示:

    MMOVF32 MR2, #5.0L    

MMOV32 @_God,MR2

在TASK2中改变God的值,如下所示:

   MMOVF32 MR2, #5.52L    

MMOV32 @_God,MR2

通过WATCHWIDOW中刷新,发现正常,God显示正常,在TASK2中将God的值变为5.0时,再次下载程序,发现God的值未改变,只有在DEBUGZ中RESET CPU后再次下载程序,发现值显示正常了,请问这是什么原因?

问题2:我在main.c文件中也定义了CNT,如下所示:

#pragma DATA_SECTION(CNT, "Cla1ToCpuMsgRAM");

volatile float CNT;

在TSAK8中完成初始化,如下所示:

    MMOVF32 MR3, #0.0L    

MMOV32 @_CNT,MR3

在TASK2中对CNT完成加1的功能:

 MADDF32  MR0, MR0, #1.0

    MMOV32  @_CNT, MR0

在WATCHWIDOW中观察CNT值显示正常,现在将

MADDF32  MR0, MR0, #1.0

    MMOV32  @_CNT, MR0这两句删去,发现CNT的值还在变化,只有RESET CPU后才归为初始化0这个值,请问这是什么原因,请教于各位高手了,小弟在此先行谢过。