This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助:F28M35调试中遇到C28工程运行停在DELAY_US(ADC_usDELAY),找不出原因



用仿真器调试,M3工程和C28工程都可以正常运行,分别进入while(1);和for(;;);循环,执行相应的中断或者其他的代码。不带仿真器上电自运行,M3正常运行,C28初始化过程中运行到 InitAdc1(); 没有向下执行,用GPIO输出作为运行位置的标志,具体定位到DELAY_US(ADC_usDELAY),之前的代码被执行,之后的代码没有执行,如果屏蔽这个DELAY_US()函数,可以正常一直执行下去。这个函数用的TI的例程,没有修改。程序中添加了

#ifdef _FLASH
memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize);
// Call Flash Initialization to setup flash waitstates
// This function must reside in RAM
InitFlash();
#endif

并且预定义“_FLASH”保证上面代码可以被执行。用仿真器全速运行和单步运行都可以顺利执行DELAY_US()。

请TI的工程师或者各位高手不吝赐教,不胜感激

  • DELAY_US(ADC_usDELAY)需要放在RAM中执行

  • 多谢你的回复,

    DELAY_US()函数定义如下

    .def _DSP28x_usDelay
    .sect "ramfuncs"

    .global __DSP28x_usDelay
    _DSP28x_usDelay:
    SUB ACC,#1
    BF _DSP28x_usDelay,GEQ ;; Loop if ACC >= 0
    LRETR

    其中.sect "ramfuncs"定义了代码段在 "ramfuncs"。在CMD文件中有如下定义,

    SECTIONS
    {/* Allocate program areas: */

    .cinit : > FLASHA PAGE = 0
    .pinit : > FLASHA, PAGE = 0
    .text : > FLASHA PAGE = 0
    codestart : > BEGIN PAGE = 0
    ramfuncs : LOAD = FLASHD,
                        RUN = RAML0,
                        LOAD_START(_RamfuncsLoadStart),
                        LOAD_SIZE(_RamfuncsLoadSize),
                        LOAD_END(_RamfuncsLoadEnd),
                        RUN_START(_RamfuncsRunStart),
                        RUN_SIZE(_RamfuncsRunSize),
                        RUN_END(_RamfuncsRunEnd),
                        PAGE = 0

    初始化过程中先执行

    memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize);

    在中间执行一些其他代码后才执行 DELAY_US()。我认为这样DELAY_US()算是在RAM中执行吧,不知道我的理解是否有误,请指教。