This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28M35 的应用情况



hai,F28M35这颗料主要是用在哪个行业的,我们希望能用来做一个带以太网口的控制系统,类似于CNC控制系统,可以同时控制几个伺服轴。前几天向TI的代理商申请样片,被建议谨慎选用,因为目前尚无客户大量使用该芯片。

请问:F28M35适合用来做CNC控制系统不,有客户大量使用F28M35的案例吗?

谢谢!

  • 我们公司也要做以太网控制系统,我现在正在调试外设过程中,网口刚调试完,正准备实验用上位机通过网口给M3发指令,M3通知C28GPIO输出端口的电平,有兴趣加我QQ:981394502  注明F28M35就好!

  • 你好!

    F28M35有18路PWM输出和3路EQEP输入,2路ADC共4个S/H单元,独立控制2-3个电机比较合适。

    因为F28M35是ARM-M3+C28的双核架构,所以非常适合有多个通讯接口需求的多电机控制系统,比如网络伺服系统。

    F28M35是才发布不久的最新的C2000系列MCU之一,所以现在使用F28M35很多都是在终端产品研发阶段。

  • 请教:

           如果是用于多伺服电机控制,最好能将ethercat或powerlink集成进来,这样应用就太有竞争力了。

          不知F28M35是否支持这些实时以太网协议?

    谢谢!