This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如题
支持!
Eric
谢谢,但是我为什么下载的最新的CCS显示的是win32的格式呢?如:CCS5.5.0.00077_win32,这就是最新的啊,没有看到win64啊。您确定可用吗?
32位的程序是可以装在64位的系统上的:
http://processors.wiki.ti.com/index.php/Windows_8_CCS
您好!我下了CCS5。5安装后它的编译器是6.2.0的,可是新版的motorware中的例程是6.2.3的,编译时有个warring. 我去哪找到6.2.3的编译器,并且如何安装呢?
现在的motorware例程全是用编译器6.2.3写的,可是ccs5.5 是6.2.0的编译器。我去哪进而下这个6.2.3,并且如何安装上去?
yanzhen
使用6.2.0编译也是没问题的。
另外可以使用CCS的help 菜单,check for update来实现更新。
感谢。是不是说,5。1版的,是不是可以通过check for update来升到5.5呢?
yanzhen.
v5.5之前的版本升级都可以用check for update来升级。但是V5.5需要到官网下载安装包进行升级。