This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于DSP 28335的SPI接口的问题:



我现在需要向DSP的SPI 的FIFO一次性写三个字节的数据,总共24bit

如我下面的代码所示:

首先片选拉低,然后写入数据,然后等待数据写完,然后片选拉高

这里出现一个问题,

就是写完数据且等待它写完之后再拉高片选时,用示波器测试发现片选拉高了之后,SPI仍然还在写数据

如果不加入我代码里面的那个delay(5)的延时,则会有大概8个脉冲在片选拉高之后

百思不得其解,请高手帮帮忙。谢谢

关于这个问题可以参考我在21IC的DSP板块发表的求助帖子。

bbs.21ic.com/forum.php

void DSP_DA()//通过SPI输出24个bit到AD5360
{

AD_CS=0;
SpiaRegs.SPITXBUF=DA_Data[0];
SpiaRegs.SPITXBUF=DA_Data[1];
SpiaRegs.SPITXBUF=DA_Data[2];
while(SpiaRegs.SPIFFTX.bit.TXFFST!=0){}
delay(3);
AD_CS=1;

}