This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

两片dsp之间epwm时基如何同步,具体该如何配置?



我想对两片DSP28035的epwm时基进行同步。我的想法是第一片DSP在epwm1 TBCTR=0时,发出同步脉冲,由GPIO33(配置为epwmsynco)输出同步脉冲信号;第二片DSP的GPIO32(配置为epwmsynci)接受同步信号输入。

按datasheet上介绍,首先,我设置第一片dsp芯片的EPwm1Regs.TBCTL.bit.SYNCOSEL = TB_CTR_ZERO,

同时配置第一片dsp的GPIO33为epwmsynco同步信号输出(GpioDataRegs.GPBCLEAR.bit.GPIO33 = 1;EALLOW;GpioCtrlRegs.GPBPUD.bit.GPIO33 = 1;EDIS;GpioCtrlRegs.GPBMUX1.bit.GPIO33 = 2;);

但是示波器观察,GPIO33没有信号输出。所以后续的第二片DSP就没有办法得到同步信号输入了。

不知道若想将epwmsynco输出到dsp外部,应该怎么样配置?