This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28m35 Ecap捕捉PWM时,如何设置可以使上升沿和下降沿同时触发一个中断ECAP1_INT



Ecap捕捉PWM时,单独捕捉上升沿或者单独捕捉下降沿都能够触发中断,怎么设置同时捕捉上升沿和下降沿,触发一个中断ECAP1_INT?

   ECap1Regs.ECEINT.bit.CEVT1 = 1;            // 1st events = interrupt
   ECap1Regs.ECEINT.bit.CEVT2 = 1;            // 2st events = interrupt

两个单独使用时,第一个下降沿触发,第二个上升沿触发,同时使用时,也只有下降沿触发,怎么才能使上升沿和下降沿同时中断?