This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CANboot烧写FLASH



最近想用CAN下载和升级程序,但28069直接通过引脚确定引导模式中没有CANboot,要选择CANboot必须配合OTP_KEY,OTP_BMODE两个存储器的值选择。

这两个存储器赋完值后应该是改不了的,那岂不是每次复位后都得调用bootloader?

还有一个问题就是通过bootloader将程序下到RAM里面的,但我编译时采用的FLASH.CMD,且在上电调用bootloader程序是固化在bootrom中的,难道在调用bootloader时候会自动调用API来烧写FLASH?如果自己编写bootloader程序,肯定是要在里面添加调用API函数,但在烧写到FLASH的段不是连续的,比如在0x3F7FF6-0x3F7FF7处就放一个长调用指令,还有一些未初始化的段,是不是直接就写到ram里就行了?

在下是新手,学DSP没多久,忘诸位高手多多指教!