Part Number: TMS320F280049
F280049芯片要求EPWM3和EPWM4同步,不和EPWM1,EPWM2同步,是否可以做到?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F280049
F280049芯片要求EPWM3和EPWM4同步,不和EPWM1,EPWM2同步,是否可以做到?
谢谢,这样也是一种方法,我的想法是把EPWM3和EPWM4这两个移到EPWM4和EPWM5两个功能脚上,那样同步起来是不是更方便一些?
Hi,
同步信号链和PWM输出是两个不同的概念。
另一种更简单的同步方式是:
EXTSYNCIN1是上升沿触发的信号。如果您的EPWM3可以确定一个固定的上升时刻的话(比如CTR = 0),将EPWM3的输出直接作为EXTSYNCIN1或EXTSYNCIN2的输入信号,也可以实现同步。
感谢回复,可能我的问题没有描述清楚,我现在要求输出4组PWM,要求EPWM1和EPWM2同步,然后另外两组我就用EPWM4和EPWM5,也可以很方便实现EPWM4和EPWM5同步,EPWM1,2和EPWM4,5不同步,之前用的是EPWM3和EPWM4,感觉不太好同步。
不客气,从器件设计来讲,3&4同步确实不如1&2同步以及4&5同步方便。