This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我现在就是一个简单的测试程序,malloc两个字节的空间,-heap 0x1000,在device simulator下可以运行通过,
但是将程序连到f2812运行时就跑飞了,这是为什么?还有我还想请教的是在2812上可以用malloc函数吗?因为在ccs3.1
中help,输入malloc回车就出现下面一段话,求解释:
The following table summarizes the TI C-Language Run-time Support Library functions that may be referenced by eXpressDSP-compliant algorithms.
Allowed or disallowed Category Typical functions in category Notes
allowed String functions strcpy, strchr, ? 1
allowed Memory-moving functions memcpy, memmove, memset, ... 2
allowed Integer math support _divi, _divu, _remi, _remu, ... 2
allowed Floating point support _addf, _subf, _mpyf, _divf, _addd, _subd, _mpyd, _divd, log10, cosh, ... 2, 3
allowed Conversion functions atoi, ftoi, itof, ... 2
disallowed Heap management functions malloc, free, realloc, alloc, ? 5
disallowed I/O functions printf, open, read, write, ? 4
disallowed misc. non-reentrant functions printf, sprintf, ctime, ... 5, 6
Notes:
1) Exceptions: strtok is not reentrant, and strdup allocates memory with malloc.
2) Some of these are issued by the compiler automatically for certain C operators.
3) The errno paradigm isn't reentrant. Thus, errno must not be used by eXpressDSP-compliant algorithms.
4) Algorithms are not allowed to perform I/O (except via DSP/BIOS APIs).
5) Algorithms must not allocate memory.
6) Algorithms must be reentrant and must, therefore, only reference reentrant functions.
See Also
Algorithm Standard rules topics
Use of DSP/BIOS API