This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

各位老师好,DSP2812 中EvaRegs的T2CNT计数器寄存器问题



各位老师好,我用DSP2812 中EvaRegs的T2CNT计数器寄存器对脉冲进行计数,计数完后,需要清零如EvaRegs.T2CNT=0;  但是通过查看并不为零,而是一个不固定的值。求老师教我解决,如何对EvaRegs的T2CNT计数器寄存器清零。谢谢

  • 我也是新手,你是配置完成后生成PWM吗?我有个配置的代码,可以完整生成PWM,只改变红色部分就能改变PWM频率和占空比;

    /****************************************************************************
    *
    *文件名:DSP28_Ev.c
    *
    *功  能:2812事件管理器的初始化函数,包括了EVA和EVB的初始化
    *
    *作  者:
    *
    ****************************************************************************/

    #include "DSP28_Device.h"

    /****************************************************************************
    *
    *名    称:InitEv()
    *
    *功    能:初始化EVA或者EVB,本例中EVA和EVB均产生占空比为40%PWM波形,EVA下面的
    *          定时器均工作于连续增模式,而EVB下面的定时器均工作于连续增/减模式,各
    *          个全比较单元的死区时间为4.27us
    *
    *入口参数:无
    *
    *出口参数:无
    *
    ****************************************************************************/

    void InitEv(void)
    {
       
        //EVA模块
        EvaRegs.T1CON.bit.TMODE=2;        //连续增模式
        EvaRegs.T1CON.bit.TPS=1;          //T1CLK=HSPCLK/2=37.5M
        EvaRegs.T1CON.bit.TENABLE=0;      //暂时禁止T1计数
        EvaRegs.T1CON.bit.TCLKS10=0;      //使用内部时钟,T1CLK
        EvaRegs.T1CON.bit.TECMPR=1;       //使能定时器比较操作
       
        EvaRegs.T2CON.bit.TMODE=2;        //连续增模式
        EvaRegs.T2CON.bit.TPS=1;          //T2CLK=HSPCLK/2=37.5M
        EvaRegs.T2CON.bit.TENABLE=0;      //暂时禁止T2计数
        EvaRegs.T2CON.bit.TCLKS10=0;      //使用内部时钟,T2CLK
        EvaRegs.T2CON.bit.TECMPR=1;       //使能定时器比较操作
       
        EvaRegs.GPTCONA.bit.TCOMPOE=1;    //定时器比较输出T1PWM_T1CMPR和T2PWM_T2CMPR由各自的定时器比较逻辑驱动    
        EvaRegs.GPTCONA.bit.T1PIN=1;      //低电平有效
        EvaRegs.GPTCONA.bit.T2PIN=2;      //高电平有效
        
        EvaRegs.T1PR=0x927B;              //1KHz的PWM,周期为1ms
        EvaRegs.T1CMPR=0x3A98;            //占空比为40%,低电平有效
        EvaRegs.T1CNT=0;
            
        EvaRegs.T2PR=0x927B;              //1KHz的PWM,周期为1ms
        EvaRegs.T2CMPR=0x57E4;            //占空比为40%,高电平有效
        EvaRegs.T2CNT=0;
       
        EvaRegs.COMCONA.bit.CENABLE=1;    //使能比较单元的比较操作
        EvaRegs.COMCONA.bit.FCOMPOE=1;    //全比较输出,PWM1-6引脚均由相应的比较逻辑驱动
     EvaRegs.COMCONA.bit.CLD=2;
       
        //死区时间为:4.27us
        EvaRegs.DBTCONA.bit.DBT=10;       //死区定时器周期,m=10
        EvaRegs.DBTCONA.bit.EDBT1=1;      //死区定时器1使能位
        EvaRegs.DBTCONA.bit.EDBT2=1;      //死区定时器2使能位
        EvaRegs.DBTCONA.bit.EDBT3=1;      //死区定时器3使能位
        EvaRegs.DBTCONA.bit.DBTPS=4,      //死区定时器预定标因子 Tdb=37.5M/16=2.34M
        
        EvaRegs.ACTR.all=0x0999;          //设定引脚PWM1-PWM6的动作属性
        
        EvaRegs.CMPR1=0x3A98;             //PWM1占空比为40%
        EvaRegs.CMPR2=0x3A98;             //PWM3占空比为40%
        EvaRegs.CMPR3=0x3A98;             //PWM5占空比为40%   

        //EVB模块
        EvbRegs.T3CON.bit.TMODE=1;        //连续增/减模式
        EvbRegs.T3CON.bit.TPS=1;          //T3CLK=HSPCLK/2=37.5M
        EvbRegs.T3CON.bit.TENABLE=0;      //暂时禁止T3计数
        EvbRegs.T3CON.bit.TCLKS10=0;      //使用内部时钟,T3CLK
        EvbRegs.T3CON.bit.TECMPR=1;       //使能定时器比较操作
       
        EvbRegs.T4CON.bit.TMODE=1;        //连续增/减模式
        EvbRegs.T4CON.bit.TPS=1;          //T4CLK=HSPCLK/2=37.5M
        EvbRegs.T4CON.bit.TENABLE=0;      //暂时禁止T4计数
        EvbRegs.T4CON.bit.TCLKS10=0;      //使用内部时钟,T4CLK
        EvbRegs.T4CON.bit.TECMPR=1;       //使能定时器比较操作
       
        EvbRegs.GPTCONB.bit.TCOMPOE=1;    //定时器比较输出T3PWM_T3CMPR和T4PWM_T4CMPR由各自的定时器比较逻辑驱动    
        EvbRegs.GPTCONB.bit.T3PIN=1;      //低电平有效
        EvbRegs.GPTCONB.bit.T4PIN=2;      //高电平有效
       
        EvbRegs.T3PR=0x493E;              //1KHz的PWM,周期为1ms
        EvbRegs.T3CMPR=0x1D4C;            //占空比为40%,低电平有效
        EvbRegs.T3CNT=0;
            
        EvbRegs.T4PR=0x493E;              //1KHz的PWM,周期为1ms
        EvbRegs.T4CMPR=0x2BF2;            //占空比为40%,高电平有效
        EvbRegs.T4CNT=0;
       
        EvbRegs.COMCONB.bit.CENABLE=1;    //使能比较单元的比较操作
        EvbRegs.COMCONB.bit.FCOMPOE=1;    //全比较输出,PWM7-12引脚均由相应的比较逻辑驱动
     EvbRegs.COMCONB.bit.CLD=2;
       
        //死区时间为:4.27us
        EvbRegs.DBTCONB.bit.DBT=10;       //死区定时器周期,m=10
        EvbRegs.DBTCONB.bit.EDBT1=1;      //死区定时器1使能位
        EvbRegs.DBTCONB.bit.EDBT2=1;      //死区定时器2使能位
        EvbRegs.DBTCONB.bit.EDBT3=1;      //死区定时器3使能位
        EvbRegs.DBTCONB.bit.DBTPS=4,      //死区定时器预定标因子 Tdb=37.5M/16=2.34M
        
        EvbRegs.ACTRB.all=0x0999;          //设定引脚PWM7-PWM12的动作属性
        
        EvbRegs.CMPR4=0x1D4C;             //PWM7占空比为40%d4c
        EvbRegs.CMPR5=0x1D4C;             //PWM9占空比为40%
        EvbRegs.CMPR6=0x1D4C;             //PWM11占空比为40%