This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28M35H52C1的1.2V和1.8V偏低和偏高



自己绘制的F28M35板卡,电源为外部供3.3V,使用内部产生1.2V和1.8V。101和113管脚拉低配置为内部产生1.2、1.8电压。相应的1.2V管脚外部配的是470nf电容,相应1.8V管脚外部配的是2.2uf电容(测试换过1.0和1.1uf电容)。实际测量1.2V管脚为1.1V和1.14V(两个相同的板卡),1.8V管脚均为1.9V。我看TI的相应文档中要求1.2V的范围是1.14—1.32V,1.8V的范围是1.71—1.995V。采用内部产生电压的方式是否也要符合上述电压范围要求?1.2V管脚的电压明显偏低,时候会导致芯片异常或者芯片不能工作。我目前的情况是,有时能正常启动,有时进入不正常的状态,我自己判断是以10M的时钟运行。请高手帮忙解答