This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

api error 24



我运行了ti的例程Example_Flash280x_API (2809),但是再次烧写时,产生错误 api error 24  用ccs 自带的depletion recover 出现错误说在0x00000000处就不行 。

我连上仿真器后看到flash有一个块内全部数据为0,其余正常。请教如何能挽救我的这块dsp.

  • 1:请问你的CCS版本烧写其他芯片是否正常?如果也不正常,请更换CCS版本

    2:请确认是否在烧写过程中有异常动作?异常断电?异常中止?

    3:请确认CSM区是否被覆盖?密码设置是否为全0?

    上述现象(1)可以通过更换CCS版本进行尝试;(2)(3)现象说明Flash遭到损坏。

  • 其他论坛上有这么说的:


    lash API Error #24报错,一般发生在是28xx某一flash扇区的寿命将近的时候(28系列芯片的flash烧写次数一般是1000次最少100次)。

    目前新的芯片好像寿命都有10W次

    我觉得这个也是有可能的哦;