This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28335的ADCINB通道采样干扰问题



ADC采样设计时,发现ADCINA通道采样正常,而ADCINB通道跟随SOCB信号产生一个脉冲干扰,类似于电容充放电的波形,导致ADCINB通道的值偏大。

测试条件:

1、测试ADC输入供电电压为3.3V,1.9V都是稳定的。

2、分别卸除ADCINA通道的输入电阻及ADCINB通道的输入电阻,外部输入只有100pF的电容,发现A通道的电平为0,而B通道的电平为3V,有一路甚至达到3.6V。

3、分别采用级联采样、SOCA采样、SOCB采样发现现象一致。

初步分析:

是ADCINB通道内部的采样保持存在问题,使得外部电容充电。

 

请问一下有什么方法解决这个问题呢,谢谢