This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C28345烧写程序到外部的EEPROM中



各位开发者:

    大家好。我最近在使用C28345开发程序,在CCS 5.1下调试好了程序。由于之前没有用过DSP,现在有几个问题请教:

    1. 如何把程序烧写到DSP的EEPROM中,以保证程序能够掉电不丢失,上电能够自动运行?

    2. 烧写的程序是否需要用Release版的?

    希望能推荐相关的资料和例程,谢谢。

  • 你的EEPROM是通过什么接口扩的,你可以参照BOOTROM的相应格式要求,将HEX文件写到EEPROM中,并将拨码开关拨至对应的引导方式,就可以实现程序上电自动运行了

  • BIN YAO1,你好。我的EEPROM是通过I2C扩展的,然后通过hex2000.exe生成出来一个.a00文件。这个文件该如何使用?怎么把它写到EEPROM中啊?我之前打算编写一个程序来写,但不清楚怎么把.a00文件里内容弄成一个数组?

    谢谢。